This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SPI使用GPMC_CSn1作为片选内核应该怎么修改



AM335X的SPI1只有2个片选,但我要接3个SPI从设备,使用spi1_cs0和spi1_cs1设备可以正常工作,我现在想使用GPMC_CSn1作为一个片选使用再接一个设备,下面是我修改board_am335xevm.c

SPI引脚的初始化(最后一行加入了gpmc_csn1管脚):

static struct pinmux_config spi1_pin_mux[] = {
    {"mcasp0_aclkx.spi1_sclk", OMAP_MUX_MODE3 | AM33XX_PULL_ENBL
        | AM33XX_INPUT_EN},
    {"mcasp0_fsx.spi1_d0", OMAP_MUX_MODE3 | AM33XX_PULL_ENBL
        | AM33XX_PULL_UP | AM33XX_INPUT_EN},
    {"mcasp0_axr0.spi1_d1", OMAP_MUX_MODE3 | AM33XX_PULL_ENBL
        | AM33XX_INPUT_EN},
    {"rmii1_refclk.spi1_cs0", OMAP_MUX_MODE2 | AM33XX_PULL_ENBL
        | AM33XX_PULL_UP | AM33XX_INPUT_EN},
    {"xdma_event_intr0.spi1_cs1", OMAP_MUX_MODE4 | AM33XX_PULL_ENBL
        | AM33XX_PULL_UP | AM33XX_INPUT_EN},
    {"gpmc_csn1.gpmc_csn1", OMAP_MUX_MODE0 | AM33XX_PULL_ENBL
        | AM33XX_PULL_UP | AM33XX_INPUT_EN},
    {NULL, 0},
};

SPI的初始化( .chip_select = 0和 .chip_select = 1 ,这里的片选0和1是怎么和管脚rmii1_refclk.spi1_cs0和xdma_event_intr0.spi1_cs1建立联系的?)

static struct spi_board_info spi_board_info[] = {
          {
                  .modalias = "mcp2515",
           // or "mcp2515" depending on your controller
                  .platform_data = &mcp251x_info,
                 .irq = 224,
                  .mode           =SPI_MODE_0,
                  .max_speed_hz = 10000000,
                  .bus_num = 2,
                  .chip_select = 0,
          },
};

static struct spi_board_info spi_board_info_1[] = {
          {
                  .modalias = "mcp2515",
           // or "mcp2515" depending on your controller
                  .platform_data = &mcp251x_info,
                 .irq = 223,
                  .mode           =SPI_MODE_0,
                  .max_speed_hz = 10000000,
                  .bus_num = 2,
                  .chip_select = 1,
          },
};

static struct spi_board_info spi_board_info_2[] = {
          {
                  .modalias = "mcp2515",
           // or "mcp2515" depending on your controller
                  .platform_data = &mcp251x_info,
                 .irq = 223,
                  .mode           =SPI_MODE_0,
                  .max_speed_hz = 10000000,
                  .bus_num = 2,
                  .chip_select = 2,
          },

注册SPI设备:
}static void spi1_init(int evm_id, int profile)
{
    setup_pin_mux(spi1_pin_mux);

    spi_register_board_info(spi_board_info,
            ARRAY_SIZE(spi_board_info));

    spi_register_board_info(spi_board_info_1,
            ARRAY_SIZE(spi_board_info_1));

    spi_register_board_info(spi_board_info_2,
            ARRAY_SIZE(spi_board_info_2));


    return;
};

但内核启动后只打印了SPI2.0和SPI2.1,没有SPI2.2

请问我该怎么样扩展SPI的片选?