This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6655: 双浮点计算

Part Number: TMS320C6655


TMS320C6655的双浮点乘加运算能力怎么样?

  • 请参考数据手册 的说明

    Section 1.3  -  "The C66x core can execute 8 single-precision floating-point MAC operations per cycle, perform double- and mixed-precision operations, and be IEEE 754 compliant."

    Section 6.25  - "Each C66x .M unit also includes IEEE floating-point multiplication operations from the C674x DSP, which includes one single-precision multiply each cycle and one double-precision multiply every 4 cycles. There is also a mixed-precision multiply that allows multiplication of a single-precision value by a double-precision value and an operation allowing multiplication of two single-precision numbers resulting in a double-precision number. The C66x DSP improves the performance over the C674x double-precision multiplies by adding an instruction allowing one double-precision multiply per cycle and also reduces the number of delay slots from 10 down to 4. Each C66x .M unit can also perform one of the following floating-point operations each clock cycle: one, two, or four single-precision multiplies or a complex single-precision multiply."