This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-J722S: .D1 or .D2 uTLB lookup fault, Non-speculative load

Part Number: PROCESSOR-SDK-J722S


我们正在TDA4VEN的C75上开发毫米波雷达的应用,运行时发现C7x访问DDR_SHARED_MEM(virtual Addr 0xc0000000 physical Addr 0x900000000)的时候大概率会发生 page fault,日志如下

[C7x_1 ]    139.312399 s: access 0x7E000000u = 10000.
[C7x_1 ]    139.312418 s: access 0x7E200000u = 0.
[C7x_1 ]    139.312437 s: access 0x100000000u = ffffffff.
[C7x_1 ]    139.312458 s: access 0x102000000u = ffffffff.
[C7x_1 ]    139.312476 s: access 0x110000000u = ff7fdfff.
[C7x_1 ]    139.312496 s: access 0x112000000u = ffffdfff.
[C7x_1 ]    139.312511 s: A0 =0xa5a5a5a5a5a5a5a5 A1 =0xa5a5a5a5a5a5a5a5
[C7x_1 ]    139.312529 s: A2 =0xa5a5a5a5a5a5a5a5 A3 =0xa5a5a5a5a5a5a5a5
[C7x_1 ]    139.312545 s: A4 =0xa5a5a5a5a5a5a5a5 A5 =0xa5a5a5a5a5a5a5a5
[C7x_1 ]    139.312561 s: A6 =0xa5a5a5a5a5a5a5a5 A7 =0xa5a5a5a5a5a5a5a5
[C7x_1 ]    139.312576 s: A8 =0xa5a5a5a5a5a5a5a5 A9 =0xa5a5a5a5a5a5a5a5
[C7x_1 ]    139.312590 s: A10=0xa5a5a5a5a5a5a5a5 A11=0xa5a5a5a5a5a5a5a5
[C7x_1 ]    139.312603 s: A12=0xa5a5a5a5a5a5a5a5 A13=0xa5a5a5a5a5a5a5a5
[C7x_1 ]    139.312616 s: A14=0xa5a5a5a5a5a5a5a5 A15=0xa5a5a5a5a5a5a5a5
[C7x_1 ]    139.312629 s: 
[C7x_1 ]    139.312636 s: Exception at 0xa5a5a5a5ada0ba50
[C7x_1 ]    139.312647 s: TSR at time of exception: 0xa5a5a5a50300ff03
[C7x_1 ]    139.312660 s: Page fault:
[C7x_1 ]    139.312669 s:   IERR=0x0000000000000001
[C7x_1 ]   IEAR=0x00000000c0000000
[C7x_1 ]   IESR=0x0000000000010845
[C7x_1 ]    139.312688 s:   Page fault exception:
[C7x_1 ]    139.312700 s:     .D1 or .D2 uTLB lookup fault, Non-speculative load
[C7x_1 ]    139.312713 s:     utlb_rstatus=0x845

另外C7x初始化mem的时候也会小概率的发生这个问题

[C7x_2 ]      7.204146 s: CIO: Init ... Done !!!
[C7x_2 ]      7.204165 s: CPU is running FreeRTOS
[C7x_2 ]      7.204177 s: APP: Init ... !!!
[C7x_2 ]      7.204187 s: SCICLIENT: Init ... !!!
[C7x_2 ]      7.204246 s: SCICLIENT: DMSC FW version [10.1.6--v10.01.06 (Fiery Fox)]
[C7x_2 ]      7.204264 s: SCICLIENT: DMSC FW revision 0xa  
[C7x_2 ]      7.204277 s: SCICLIENT: DMSC FW ABI revision 4.0
[C7x_2 ]      7.204290 s: SCICLIENT: Init ... Done !!!
[C7x_2 ]      7.204302 s: UDMA: Init ... !!!
[C7x_2 ]      7.204328 s: UDMA: Init ... Done !!!
[C7x_2 ]      7.204340 s: MEM: Init ... !!!
[C7x_2 ]      7.204375 s: A0 =0xa5a5a5a5a5a5a5a5 A1 =0xa5a5a5a5a5a5a5a5
[C7x_2 ]      7.204391 s: A2 =0xa5a5a5a5a5a5a5a5 A3 =0xa5a5a5a5a5a5a5a5
[C7x_2 ]      7.204405 s: A4 =0xa5a5a5a5a5a5a5a5 A5 =0xa5a5a5a5a5a5a5a5
[C7x_2 ]      7.204418 s: A6 =0xa5a5a5a5a5a5a5a5 A7 =0xa5a5a5a5a5a5a5a5
[C7x_2 ]      7.204431 s: A8 =0xa5a5a5a5a5a5a5a5 A9 =0xa5a5a5a5a5a5a5a5
[C7x_2 ]      7.204445 s: A10=0xa5a5a5a5a5a5a5a5 A11=0xa5a5a5a5a5a5a5a5
[C7x_2 ]      7.204458 s: A12=0xa5a5a5a5a5a5a5a5 A13=0xa5a5a5a5a5a5a5a5
[C7x_2 ]      7.204471 s: A14=0xa5a5a5a5a5a5a5a5 A15=0xa5a5a5a5a5a5a5a5
[C7x_2 ]      7.204484 s: 
[C7x_2 ]      7.204492 s: Exception at 0xa5a5a5a5b1a3fb60
[C7x_2 ]      7.204504 s: TSR at time of exception: 0xa5a5a5a50300ff03
[C7x_2 ]      7.204516 s: Page fault:
[C7x_2 ]      7.204525 s:   IERR=0x0000000000000001
[C7x_2 ]   IEAR=0x000000011bffffc8
[C7x_2 ]   IESR=0x0000000000010805
[C7x_2 ]      7.204542 s:   Page fault exception:
[C7x_2 ]      7.204552 s:     .D1 or .D2 uTLB lookup fault, Non-speculative load
[C7x_2 ]      7.204566 s:     utlb_rstatus=0x805

还有一个问题是我尝试着用ccs去debug的时候,提示找不到xds110, 我的板子是J722SXH01EVM,尝试了重新插拔,也试了拨码开关拨到noboot/uart/sd各种启动模式,插上usb后只有LD3亮起,LD2不亮

An error occurred while hard opening the controller.

-----[An error has occurred and this utility has aborted]--------------------

This error is generated by TI's USCIF driver or utilities.

The value is '-260' (0xfffffefc).
The title is 'SC_ERR_XDS110_OPEN'.

The explanation is:
An attempt to connect to the XDS110 failed.
The cause may be one or more of: no XDS110 is connected, invalid
firmware update, invalid XDS110 serial number, or faulty USB
cable. The firmware and serial number may be updated using the
xdsdfu utility found in the .../ccs_base/common/uscif/xds110
directory of your installation. View the XDS110SupportReadMe.pdf
file there for instructions.

[End: Texas Instruments XDS110 USB Debug Probe_0]

期待回复,多谢!