This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BCP中MOD子模块如何实现上行CQI复用,以及RI、ACK交织



本人在6670上调试PUSCH链路,BCP中MOD子模块对上行CQI复用,以及RI、ACK交织处理过程不太清楚。有以下几个问题想请教各位大神。非常感谢!!!

(1)BCP中MOD子模块中的软调制与硬调制有何区别?

(2)要进行上行数据信息调制及UCI信息复用、交织,MOD的几个寄存器值该怎么设置(特别哪些字段的值要注意)?

(3)MOD子模块输出时,是不是将CQI、RI、ACK信息位置填充虚比特??

  • 你的问题在bcp user guide中都有,参考BCP user guide有对软调制及硬调制的使用场景说明,软调制是在LTE PUSCH PIC/SIC使用,应调制用于LTE PDSCH,如果是处理PUSCH,建议使用软调制,可以支持加扰、调制及交织。设置ACK/RI/CQI长度即可;对CQI/RI/ACK位置填充dummy bit对应-127对应0x81.

  • TI的BCP测试例程中,测试下行PDSCH流程代码中,调制完后12600收据完全正确。在这基础上我修改成软调制模式,OFDM符号数,CQI数三个参数。

    但调制(QPSK)输出来的数据不对,长对只有628。数据也不太对,中间还有值为0。不知道是哪里的问题。(是不是信道类型必须设置为PUSCH??),希望你能再帮忙看看,再次感谢!!