This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VM: 在我的自定义板子上我使用SDK版本10.01.00.04的Yocto生成的 tiboot3.bin出现不能正常刷写的错误

Part Number: TDA4VM


在我的自定义板子上我使用SDK版本10.01.00.04的Yocto生成的 tiboot3.bin出现不能正常刷写的错误,错误如下;

tiboot3.bin刷写完成后刷写sysfw.itb

此时本来应该出现但是dfu设备已经没有了。

tda4vm的串口终端出现提示:

我已经确定了我的自定义设备在ti-processor-sdk-linux-j7-evm-08_06_00_11也就是sdk的08_06_00_11版本可以的刷写但是我现在升级了到了10_01_00_04却不能正常刷写,我已经确定了我的硬件前后没有任何改动。

下面是08_06_00_11版本下刷写成功的串口终端打印;(其他步骤均一致)

我想知道从08_06_00_11到10_01_00_04对于sysfw.itb  tiboot3.bin  tispl.bin  u-boot.img的改变,和不能刷写的原因。