This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dm8127 CMOS接口驱动问题



请问DM8127IPNC 的RDK包里有MN34041的sensor 配 LVDS324使用。请问原代码LVDS324的驱动部分或初如化部分代码在哪个文件里?

还有DM8127IPNC样机有提供支持CSI接口,比如用松下MN34229是否可直接接CSI串行接口,驱动如何配置?当然有支持LVDS324串转并桥接的并行接口,这两种接口,哪一个性能优势好?

  • lu xinjian 说:

    请问DM8127IPNC 的RDK包里有MN34041的sensor 配 LVDS324使用。请问原代码LVDS324的驱动部分或初如化部分代码在哪个文件里?

    【Chris】请参考uboot里面的I2C命令。

    lu xinjian 说:

    还有DM8127IPNC样机有提供支持CSI接口,比如用松下MN34229是否可直接接CSI串行接口,驱动如何配置?当然有支持LVDS324串转并桥接的并行接口,这两种接口,哪一个性能优势好?

    【Chris】我在网上看到的MN34229PL是subLVDS的接口不是CSI的。你确认MN34229有支持CSI的型号么?如果是,驱动只能参考目前驱动支持的CSI sensor的相关部分。

  • subLVDS是lvds差分接口,看appro接供的原理图的接口也是走差分线。这两种接口是区别?

    还有uboot里面的i2c的命令是什么,能否具体说明一点,多谢!

  • 你好,

    subLVDS和CSI都是差分信号,但是是不同的标准。DM8127支持的是CSI。

    请参考下面的bootcmd里面的i2c命令,就是配置LVDS324的命令。

    setenv bootcmd 'i2c dev 2;i2c write 0x2d 9 0x0a;i2c write 0x2d 0xa 0x62;ipnc_ff_init 1;nboot 0x81000000 0 0x280000; bootm';saveenv