This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6670上的多个EDMA同时运行的问题



我使用KI的例程改编了EDMA的拷贝,实现了EDMA的中断。但是当我同时发起多个EDMA(代码中是32个EDMA1)的时候,如果中断(EDMA0_ISR,EDMA1_ISR,EDMA2_ISR)中不加入打印语句printf("%x in ISR1\n", *TPCC_IPR);那么我的测试函数shadow_edma_test()中的统计进入中断次数的变量cnt_18[18]里面是{2,1,1,1,1,。。。。。。},说明只有EDMA1_0进入了一次,其他的EDMA都无法进入,但是当我把打印语句printf("%x in ISR1\n", *TPCC_IPR);这一行取消注释,可以看到cnt_18[18]里面都是相同的进入中断的次数,而且也可以不停打印该语句。

请帮我看看代码里面有什么问题,导致出现这样的现象。谢谢了

bsp_6670_csl.rar