硬件:AM335X ICE V2.1A
load TMDXICE3359_v2_1A.gel出现错误如下:
progress .......
CortxA8: Output: DDR PHY DATA0 Register configuration is in progress .......
CortxA8: Output: DDR PHY DATA1 Register configuration is in progress .......
CortxA8: Output: Setting IO control registers.......
CortxA8: Output: EMIF Timing register configuration is in progress .......
CortxA8: Trouble Writing Memory Block at 0x4c0000e4 on Page 0 of Length 0x4: (Error -1065 @ 0x3D5A) Unable to access device memory. Verify that the memory address is in valid memory. If error persists, confirm configuration, power-cycle board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.14.5)
AM3359_ICE_Initialization() cannot be evaluated.
Target failed to write 0x4C0000E4
at *((unsigned int *) (0x4C000000+0x0E4))=(unsigned int) 0x07 [TMDXICE3359_v2_1A.gel:281]
at DDR3_EMIF_Config() [TMDXICE3359_v2_1A.gel:374]
at AM3359_ICE_Initialization()
是memory坏片了?请帮分析原因,我该如何解决,谢谢。