This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Waiting for SFT on the OMAP-L138的问题

Other Parts Discussed in Thread: OMAP-L138

执行sft_OMAP-L138.exe 后一直停留在:Waiting for SFT on theOMAP-L138... ,再也不能进行下去。用BSL测试程序发现是我们的板子上面的spiflash芯片和开发板上的flash芯片的ID信息有点不太一样。我想问一下sfh_OMAP-L138.exe是否跟flash芯片的的内部ID信息有关。

  • 如果你的SPI flash跟EVM板不一样的话,需要做些修改,请参考下面的wiki网站。
    http://processors.wiki.ti.com/index.php/Serial_Boot_and_Flash_Loading_Utility_for_OMAP-L138#Modifications_for_Custom_Boards

     

  •    非常感谢你的回复。根据你推荐的文章,我对OMAP-L138进行了修改,并重新编译。整个编译环境搭好后,在cygwin中先 make clean 然后再make,发现如下错误:  C:\CCSV5_1_0\CCSv5\tools\complier\C6000\bin\c16x: 命令未找到

    我就是想问一下,为什么会出现如上错误,怎么改正。如果有人编译成功过,可不可以跟我联系一下,非常感激,项目卡在这了。我的电话是18758063749.