This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM335 u-boot为什么要设置I2C为从模式?



无论读eeprom还是PMIC,am335不应处于主模式吗?u-boot代码如下:

const struct dpll_params *get_dpll_ddr_params(void)
{
    struct am335x_baseboard_id header;

    enable_i2c0_pin_mux();
    i2c_init(CONFIG_SYS_OMAP24_I2C_SPEED, CONFIG_SYS_OMAP24_I2C_SLAVE);
    if (read_eeprom(&header) < 0)
        puts("Could not get board ID.\n");

    if (board_is_evm_sk(&header))
        return &dpll_ddr_evm_sk;
    else if (board_is_bone_lt(&header))
        return &dpll_ddr_bone_black;//400Mhz
    else if (board_is_evm_15_or_later(&header))
        return &dpll_ddr_evm_sk;//303Mhz
    else
        return &dpll_ddr;
}