This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TRF37B32: 单通道Power Down时的电流

Part Number: TRF37B32


Q: TRF37B32数据手册列出了LPM = 0时的典型电流为305 mA。它指出可以通过PDA或PDB分别关闭每个通道的电源,从而从禁用通道的IF放大器中消除偏置电流。LPM = 0且单通道Power Down时的典型电源电流是多少?

  • A: 由于power down通道的静态电流,单通道电流将高于305mA / 2 = 155mA。我将在实际设备上进行测量,然后再与您联系

    启用2个通道后,我在3.3V测得EVM上有286mA电流。启用一个通道并使用另一个PDN时,3.3V消耗156mA电流。