Part Number: AFE7769
戴工:
你好! 我们现在测试过程中,发现在DPD运行过程中存在烧PA的现象,我们想使用AFE7769的TX PA Protection功能;
请问一下这个功能怎么使用?需要怎么设置门限参数?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
李工,
PAP的功能用下面这个C function. 具体int windowCntr,int errorCntr,int threshold, 这3个参数怎么设置我们内部需要内部确认一下,这周稍后给您回复
int configSrModeMovingAvg(int fd,int ulCh,int enable,int samples,int windowCntr,int errorCntr,int threshold){
/*
ulCh: 0=TXA,1=TXB,2=TXC,3=TXD
enable: 0/1=Disable,2=JPL mode,3=Abs mode
samples: Number of samples used for moving average PAP computation. 0:32Samples,1:64Samples,2:96Samples,3:128Samples
windowCntr: Moving average window counter running at interface rate/2 clock
errorCntr: Moving average error counter running at interface rate/2 clock
threshold: Moving average mode, accumulator threshold value above which PAP will be triggered for this mode
李工,
RU enable PAP的配置文件&bringup script在此:
bringup script:
configuration file:
PAP CAPI:
/cfs-file/__key/communityserver-discussions-components-files/119/configSrModeMovingAvg.c
Example settings,
Enable = 2 # JPL approximation
Samples = 0 // indicating 32 samples
windowCntr = 256
errorCntr = 16
threshold = 2560 (please check below lines for threshold calculation)
threshold_in_dBFS=-10 # dBFs
thr=int(32768*pow(10,threshold_in_dBFS/20.))
另外戴工,贵司的现在AFE7769D的自带DPD功能,现在在60W输出功率的情况下可以做到多少ACPR?前些天ADI这边发了一个3.5G的80W的功率的,用他们芯片自带DPD,ACPR可以做到-47dBc
我们测过3.85GHz FDD 56w BW 200MHz, 您提到的这个use case目前还没有测过. 如果需要提供AFE7769D的ACLR数据,需要你们跟TI-Sales签个NDA才能给.