This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AFE7769: AFE7769的FB通道功率问题

Part Number: AFE7769


戴工:

    你好! 我们在低温40度时,发现AFE7769的FB通道的功率出现异常?这个现象怀疑时AFE7769带来的,因为如果带电工作,设备降低到-40度时FB通道读取的功率还算正常

但是如果不带电,将设备放到低温箱然后降温到-40度再启动,就会出现FB通道读取的功率极其微弱,此时如果温度上升到-30,或者PCB工作一段时间重启PCB也可以正常。

   想问一下,FB通道AFE7769可以直接读取功率吗?(我们现在FB通道的功率读取时通过FPGA那边计算出来的,异常时,CHECK7769的204B都正常,未发现异常)