TRF370417EVM参考板原理图上的BBIP、BBIN和BBQP、BBQN没有外接50欧姆电阻到地,实际使用时如果是罗德SMW200A信号源输出的IQ baseband接到参考板baseband input,罗德SMW200A信号源输出IQ baseband信号是电流信号,参考板的baseband input没有电阻到地,那电流如何转化为电压信号?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TRF370417EVM参考板原理图上的BBIP、BBIN和BBQP、BBQN没有外接50欧姆电阻到地,实际使用时如果是罗德SMW200A信号源输出的IQ baseband接到参考板baseband input,罗德SMW200A信号源输出IQ baseband信号是电流信号,参考板的baseband input没有电阻到地,那电流如何转化为电压信号?

如果提供给TRF370417EVM参考板的BBIP、BBIN和BBQP、BBQN管脚是电压信号,那是不是参考板的BBIP、BBIN和BBQP、BBQN管脚不需要下拉电阻到地?
SMW200A输出的IQ信号差分阻抗是100欧姆,输出的是电压信号,可以配置输出电压信号偏置为0V到4V,单端电压信号摆幅为0.01V到1V
如果提供给TRF370417EVM参考板的BBIP、BBIN和BBQP、BBQN管脚是电压信号,那是不是参考板的BBIP、BBIN和BBQP、BBQN管脚不需要下拉电阻到地?
对的,不需要。