Part Number: IWR6843AOP
Other Parts Discussed in Thread: SN74LVC8T245, , SN74AVC4T245
我现在有一款基于IWR6843AOP定制的雷达板,我的VIO供电电平为1.8V,请问该雷达芯片是否有驱动电流的要求,因为我的URAT的电平为3.3V,所以通过UART与雷达进行数据交互的地方有电平转换的芯片,其中3.3V转1.8V的芯片是SN74AVC4T245,驱动电流最大为8mA,当我输入3.3V的高电平或者输入低电平时,输出引脚始终为1.8V的高电平。1.8V转3.3V的芯片是SN74LVC8T245,驱动电流最大为24mA,雷达输出的信号能经过电平转换为3.3V的信号。所以我想请问一下我的3.3V转1.8V的电平转换芯片是不是因为驱动能力不够,IWR6843AOP芯片本身的IO接口是否有驱动能力的要求。
期待您的回复!谢谢!