This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA302: pga302芯片采集到的padc是一个固定值,不会改变

Part Number: PGA302


在大批量生产过程中,发现有部分pga302芯片采集到的padc是一个固定值,不会变化,换一个芯片可以解决此问题。

对比了有问题的芯片与正常芯片,eep部分除系数外,其他数据一样。

;GRID_EEPROM_MEMSPACE
0x00 H0 [7:0],D0
0x01 H0 [15:8],0D
0x02 H1 [7:0],00
0x03 H1 [15:8],00
0x04 H2 [7:0],00
0x05 H2 [15:8],00
0x06 H3 [7:0],00
0x07 H3 [15:8],00
0x08 G0 [7:0],E5
0x09 G0 [15:8],C4
0x0A G1 [7:0],00
0x0B G1 [15:8],00
0x0C G2 [7:0],00
0x0D G2 [15:8],00
0x0E G3 [7:0],00
0x0F G3 [15:8],00
0x10 N0 [7:0],37
0x11 N0 [15:8],64
0x12 N1 [7:0],00
0x13 N1 [15:8],00
0x14 N2 [7:0],00
0x15 N2 [15:8],00
0x16 N3 [7:0],00
0x17 N3 [15:8],00
0x18 M0 [7:0],00
0x19 M0 [15:8],00
0x1A M1 [7:0],00
0x1B M1 [15:8],00
0x1C M2 [7:0],00
0x1D M2 [15:8],00
0x1E M3 [7:0],00
0x1F M3 [15:8],00
0x20 PADC_GAIN,01
0x21 TADC_GAIN,01
0x22 PADC_OFFSET [7:0],11
0x23 PADC_OFFSET [15:8],01
0x24 TADC_OFFSET [7:0],00
0x25 TADC_OFFSET [15:8],00
0x26 P_GAIN_SEL,06
0x27 T_GAIN_SEL,2A
0x28 TEMP_SW_CTRL,08
0x29 OFFSET_CANCEL,00
0x2A DAC_FAULT_MSB,00
0x2B A0,00
0x2C A1 [7:0],00
0x2D A1 [15:8],00
0x2E A2 [7:0],00
0x2F A2 [15:8],00
0x30 B1 [7:0],00
0x31 B1 [15:8],00
0x32 NORMAL_LOW [7:0],00
0x33 NORMAL_LOW [15:8],00
0x34 NORMAL_HIGH [7:0],FF
0x35 NORMAL_HIGH [15:8],3F
0x36 LOW_CLAMP [7:0],00
0x37 LOW_CLAMP [15:8],00
0x38 HIGH_CLAMP [7:0],FF
0x39 HIGH_CLAMP [15:8],3F
0x3A DIAG_BIT_EN,00
0x3B SERIAL_NUMBER [7:0],00
0x3C SERIAL_NUMBER [15:8],00
0x3D SERIAL_NUMBER [23:16],00
0x3E SERIAL_NUMBER [31:24],00
0x3F EEPROM_CRC,00
EOF
;GRID_EEPROM_MEMSPACE
0x00 H0 [7:0],F4
0x01 H0 [15:8],1F
0x02 H1 [7:0],00
0x03 H1 [15:8],00
0x04 H2 [7:0],00
0x05 H2 [15:8],00
0x06 H3 [7:0],00
0x07 H3 [15:8],00
0x08 G0 [7:0],41
0x09 G0 [15:8],A8
0x0A G1 [7:0],00
0x0B G1 [15:8],00
0x0C G2 [7:0],00
0x0D G2 [15:8],00
0x0E G3 [7:0],00
0x0F G3 [15:8],00
0x10 N0 [7:0],F0
0x11 N0 [15:8],FB
0x12 N1 [7:0],00
0x13 N1 [15:8],00
0x14 N2 [7:0],00
0x15 N2 [15:8],00
0x16 N3 [7:0],00
0x17 N3 [15:8],00
0x18 M0 [7:0],00
0x19 M0 [15:8],00
0x1A M1 [7:0],00
0x1B M1 [15:8],00
0x1C M2 [7:0],00
0x1D M2 [15:8],00
0x1E M3 [7:0],00
0x1F M3 [15:8],00
0x20 PADC_GAIN,01
0x21 TADC_GAIN,01
0x22 PADC_OFFSET [7:0],11
0x23 PADC_OFFSET [15:8],01
0x24 TADC_OFFSET [7:0],00
0x25 TADC_OFFSET [15:8],00
0x26 P_GAIN_SEL,06
0x27 T_GAIN_SEL,2A
0x28 TEMP_SW_CTRL,08
0x29 OFFSET_CANCEL,00
0x2A DAC_FAULT_MSB,00
0x2B A0,00
0x2C A1 [7:0],00
0x2D A1 [15:8],00
0x2E A2 [7:0],00
0x2F A2 [15:8],00
0x30 B1 [7:0],00
0x31 B1 [15:8],00
0x32 NORMAL_LOW [7:0],00
0x33 NORMAL_LOW [15:8],00
0x34 NORMAL_HIGH [7:0],FF
0x35 NORMAL_HIGH [15:8],3F
0x36 LOW_CLAMP [7:0],00
0x37 LOW_CLAMP [15:8],00
0x38 HIGH_CLAMP [7:0],FF
0x39 HIGH_CLAMP [15:8],3F
0x3A DIAG_BIT_EN,00
0x3B SERIAL_NUMBER [7:0],00
0x3C SERIAL_NUMBER [15:8],00
0x3D SERIAL_NUMBER [23:16],00
0x3E SERIAL_NUMBER [31:24],00
0x3F EEPROM_CRC,00
EOF