Part Number: IWR1843
硬件:IWR1843,SDK:mmwave_sdk_03_06_02_00-LTS,代码:out_of_box_18
问题:这是从可视化工具下载的4RX-1TX的参数配置,我只对配置在红框处的参数进行修改,目的是对chirp进行移相,使得chirp间相位差为180,现在这个配置无法启动雷达,我加多一个profileCfg配置雷达就无法启动,请问这是为什么呢?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
你的phaseshifter 字段为180. 变量txPhaseShiter的定义如下,如果赋值180的话,并非180°的含义。

官方的BPM的demo 请参考
Thanks
Ken