This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3005: OPT3005在IR LED旁會量測到亮度

Part Number: OPT3005


Hi 

日前PCB將OPT3005放在IR LED旁(如下圖),在暗房未開啟IR LED(850nm)量測到亮度值為0,

,但開啟IR LED(850nm)後卻量測到亮度值約為12左右,看規格書應該是不會偵測到IR LED的亮度值才對?

另外請問Full-Scale Range(E3~E0)可以手動設定嗎?