您好,
我想用AWR2944网口将做完二维FFT的RDM图输出出来,我的波形配置是距离维512格*32chirp*16通道(4发4收),对应一帧RDM图是2MB。首向我想问一下有什么接口可以获取到这个RDM图吗?其次我目前担心AWR2944的片载内存是否支持用网口传输这么大数据?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
一帧RD为2MB,假设帧周期为50ms,那么以太网的数据流量为2(MB)*20(FPS)*8=320Mbps,
AWR2944的以太网速率仅为100Mbps,因此无法传输。建议使用LVDS传输RD数据。
参考
Thanks
Ken