IWR6843ISK: The IWR6843ISK cannot be used on the Linux system.

Part Number: IWR6843ISK
Other Parts Discussed in Thread: IWR6843

We were able to successfully connect and run the system on the Windows platform using USB and IWR6843ISK. However, when we connected the IWR6843ISK to the Linux system via USB, it failed to function properly and couldn't receive data. Moreover, the LED lights were different. On the LED light circled in blue on the Windows system, it would go out after a while, but on the Linux system, it remained on and didn't go out.

e81f9e22217b62340404355442484083.jpg