Part Number: AWR1642BOOST
我尝试利用tiradar.ConfigFile = "C:\Configs\ xwr68xx_2Tx_BestRange_UpdateRate_10.cfg";修改我的配置文件,但是当cmd出现success后我的dca1000左上角的灯没有闪烁,我对串口的配置进行了筛查,对于默认的cfg:发送 [30]: sensorStart -> 回复: Debug: Init Calibration Status = 0x17fe
*** 警告: sensorStart 可能失败 (Status = Debug: Init Calibration Status = 0x17fe) ***
-> 回复: Done
对于我的配置cfg,发送 [30]: sensorStart -> 回复: Exception: ./mss/mmw_cli.c, line 282.
*** 警告: sensorStart 可能失败 (Status = Exception: ./mss/mmw_cli.c, line 282.) ***有时时erroe -1以下是默认cfg和我配置的
默认:
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 3 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
profileCfg 0 77 429 7 57.14 0 0 70 1 256 5209 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
frameCfg 0 1 16 0 100 1 0
lowPower 0 1
guiMonitor -1 0 0 0 0 0 0
cfarCfg -1 0 2 8 4 3 0 15 1
cfarCfg -1 1 0 4 2 3 1 15 1
multiObjBeamForming -1 1 0.5
clutterRemoval -1 0
calibDcRangeSig -1 0 -5 8 256
extendedMaxVelocity -1 0
bpmCfg -1 0 0 1
lvdsStreamCfg -1 0 1 0
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
CQRxSatMonitor 0 3 5 121 0
CQSigImgMonitor 0 127 4
analogMonitor 0 0
aoaFovCfg -1 -90 90 -90 90
cfarFovCfg -1 0 0 8.92
cfarFovCfg -1 1 -1 1.00
calibData 0 0 0
sensorStart
我的:
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 3 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
profileCfg 0 77 5 6 83 0 0 48 1 256 3430 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
frameCfg 0 1 16 0 100 1 0
lowPower 0 0
guiMonitor -1 0 0 0 0 0 0
cfarCfg -1 0 2 8 4 3 0 15 1
cfarCfg -1 1 0 4 2 3 1 15 1
multiObjBeamForming -1 1 0.5
clutterRemoval -1 0
calibDcRangeSig -1 0 -5 8 256
extendedMaxVelocity -1 0
bpmCfg -1 0 0 1
lvdsStreamCfg -1 1 1 0
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
CQRxSatMonitor 0 3 5 121 0
CQSigImgMonitor 0 127 4
analogMonitor 0 0
aoaFovCfg -1 -90 90 -90 90
cfarFovCfg -1 0 0 8.92
cfarFovCfg -1 1 -1 1.00
calibData 0 0 0
sensorStart
请问哪里有问题,另外我是通过AWR1642BOOST给dca1000供电的,我经常会出现采集了一次,过段时间就会出现连接报错,只有我断电重启才能使用。
I tried to modify my configuration file using `tiradar.ConfigFile = "C:\\Configs\\xwr68xx_2Tx_BestRange_UpdateRate_10.cfg"`. However, after the cmd displayed "success", the indicator light in the upper left corner of the DCA1000 did not blink. I checked the serial port configuration.
For the **default cfg**:
When sending `[30]: sensorStart`, the response is:
`Debug: Init Calibration Status = 0x17fe`
*** Warning: sensorStart may have failed (Status = Debug: Init Calibration Status = 0x17fe) ***
-> Response: Done
For **my customized cfg**:
When sending `[30]: sensorStart`, the response is:
`Exception: ./mss/mmw_cli.c, line 282.`
*** Warning: sensorStart may have failed (Status = Exception: ./mss/mmw_cli.c, line 282.) ***
Sometimes an **error -1** is returned.
Below are the default cfg and my customized cfg:
**Default cfg**:
```
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 3 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
profileCfg 0 77 429 7 57.14 0 0 70 1 256 5209 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
frameCfg 0 1 16 0 100 1 0
lowPower 0 1
guiMonitor -1 0 0 0 0 0 0
cfarCfg -1 0 2 8 4 3 0 15 1
cfarCfg -1 1 0 4 2 3 1 15 1
multiObjBeamForming -1 1 0.5
clutterRemoval -1 0
calibDcRangeSig -1 0 -5 8 256
extendedMaxVelocity -1 0
bpmCfg -1 0 0 1
lvdsStreamCfg -1 0 1 0
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
CQRxSatMonitor 0 3 5 121 0
CQSigImgMonitor 0 127 4
analogMonitor 0 0
aoaFovCfg -1 -90 90 -90 90
cfarFovCfg -1 0 0 8.92
cfarFovCfg -1 1 -1 1.00
calibData 0 0 0
sensorStart
```
**My customized cfg**:
```
sensorStop
flushCfg
dfeDataOutputMode 1
channelCfg 15 3 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
profileCfg 0 77 5 6 83 0 0 48 1 256 3430 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 2
frameCfg 0 1 16 0 100 1 0
lowPower 0 0
guiMonitor -1 0 0 0 0 0 0
cfarCfg -1 0 2 8 4 3 0 15 1
cfarCfg -1 1 0 4 2 3 1 15 1
multiObjBeamForming -1 1 0.5
clutterRemoval -1 0
calibDcRangeSig -1 0 -5 8 256
extendedMaxVelocity -1 0
bpmCfg -1 0 0 1
lvdsStreamCfg -1 1 1 0
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
CQRxSatMonitor 0 3 5 121 0
CQSigImgMonitor 0 127 4
analogMonitor 0 0
aoaFovCfg -1 -90 90 -90 90
cfarFovCfg -1 0 0 8.92
cfarFovCfg -1 1 -1 1.00
calibData 0 0 0
sensorStart
```
In addition, I power the DCA1000 via the AWR1642BOOST. I often encounter a connection error after one round of data collection; the only solution is to power off and restart the device.