Part Number: DCA1000EVM
Hi,I want to control multiple DCA1000EVMs for data acquisition through a PC. The specific approach is to connect two DCA1000EVMs to a PC and configure their IP addresses, MAC addresses, and port numbers using the CLI tool. I created two instantiated consoles. Both consoles can connect to their respective DCA1000EVMs. However, when I send a capture command to the first DCA1000EVM from the first console using the CLI tool, and then send a capture command to the second DCA1000EVM from the second console using the CLI tool, the first DCA1000EVM works normally while the second DCA1000EVM reports an error. The result is shown in the figure below. What is the reason for this, and how can it be resolved?