This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243BOOST: 有关使用mmwave studio导出JSON文件的一些问题

Part Number: AWR2243BOOST
Other Parts Discussed in Thread: DCA1000EVM

你好,我在使用mmwave studio对AWR2243BOOST设置好参数后,导出两个JSON文件(mmwave.json和setup.json),有几个问题需要请教一下。

1、这两个文件各自的作用是什么?我看mmwave.json这个文件貌似是配置好参数后根据参数自动生成的。

2、这个mmwave.json与使用CLI工具时给DCA1000EVM进行配置的config.json有什么区别吗?(我也使用过CLI工具控制DCA1000EVM进行数据采集)。

3、能否在config.json中加入mmwave.json的一些参数,然后利用CLI工具通过控制DCA1000EVM给AWR2243BOOST板进行参数配置?

4、我在使用mmwave studio对AWR2243BOOST板进行参数设置时拿示波器抓了一下指令,然后自己通过编写上位机,通过自己组帧并利用SPI通信实现对AWR2243BOOST板的参数设置,对AWR2243BOOST板单个发射阵元可以进行控制,采集的数据大小也跟理论上计算得出的数量大小一致,但是在进行多个发射阵元控制时,发现采集的数量大小仍然只是一个发射阵元的,也即是说另外一个发射阵元并不能根据配置采集到数据,我通过示波器抓了一下指令,跟我自己组帧的指令一致,然后我试着用mmwave studio配置参数并导出.json文件,也即是mmwave.json与setup.json,发现mmwave.json中有多个发射阵元的配置,而我仅仅只是抓了一下指令进行组帧,会不会是因为缺少mmwave.json而导致另外一个发射阵元不工作呢?