This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWRL6432AOPEVM: Where do i find GPIO pins for SPI communication on the EVM board

Part Number: IWRL6432AOPEVM
Other Parts Discussed in Thread: MMWAVE-L-SDK, IWRL6432AOP,

I'm using CCS to add SPI module to Motion and presence detection project. So that i can send people presence, count information to an external MCU. In example.syscfg I've Added MCSPI and selected PAD_AG/D10, Aj/c11,AI/B12, AH/D11 as SPI pins. I can't find the pins on the EVM board to check the SPI signals. Can you provide me any reference documents for locating these pins.  image.png