This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: Request for Step-by-Step Procedure to Run Vital SIGNS on IWR6843AOPEVM

Part Number: IWR6843AOPEVM

Dear TI Support Team,

I am working with the IWR6843AOPEVM and attempting to run the Vital Signs demo and GUI, but I am unable to get it running successfully.

I have already gone through the available Vital Signs forum discussions and documentation links. Unfortunately, these resources are not helpful for the AOPEVM variant, as they are fragmented, incomplete, and heavily dependent on assumptions about software versions and board variants.

I would like to explicitly request that no further redirection to existing links or forum threads be provided. Instead, I kindly ask you to directly provide a clear, end-to-end, step-by-step procedure to run the Vital Signs demo on IWR6843AOPEVM.

Please include the following details in the response itself:

  1. Exact required software versions (mmWave SDK, Industrial Toolbox, MATLAB/Python, CCS, etc.)

  2. Correct Vital Signs firmware binary and flashing procedure

  3. Serial port configuration and expected COM port mapping

  4. Proper sequence to start the sensor and launch the GUI

  5. AOPEVM-specific hardware or configuration requirements

  6. Common issues that prevent the GUI from running or displaying data

At this stage, a direct procedural explanation is required rather than references to documentation, as the current links do not resolve the issue.

Thank you for your understanding and support.

Regards,
Koushik