IWR1642BOOST: IWR1642BOOST: How to synchronize frame acquisition between two radars separated by 100m?

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR1642

Hello,

We are planning to use two IWR1642BOOST boards to build a synchronized acquisition setup for a research experiment.

The two radars are separated by about 100 meters. One radar will be placed at the starting point and the other radar will be placed at the ending point. Both radars will observe the same moving target simultaneously.

We would like to align the collected data in time during post-processing.

Could you please help confirm:

1. Does IWR1642BOOST support frame-level synchronization between two boards?
2. Can SYNC_IN / SYNC_OUT be used for synchronization?
3. Is there any recommended synchronization solution for two radars separated by about 100 meters?
4. Are there any reference examples or recommended hardware connections for this setup?

Thank you.