This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP117: 请问芯片之间是否存在误差

Part Number: TMP117


用TMP117做了一个体温传感的设备,戴在同一支手臂上,发现它们测量出来的温度有所不同,有大概0.5度的差值。这个正常吗?还是会受到焊接或其他因素的影响?

  • 您好, 建议您参考datasheet Page34的8.2.2.3 Synchronized Temperature Measurements 部分的介绍:

    就是多个TMP117 测量不同地方的温度时,建议采用触发复位的方式. 控制寄存器需要配置为CC模式,转换周期为16s.四个设备采用不同的地址挂接在同一I2C总线上, 主控发生通用呼叫复位命令, 该命令触发所有设备进行复位大概需要1.5ms时间,并根据控制寄存器的配置同时触发进行温度采样. 主机有16s的时间从设备中读取数据.

    所以按照触发复位,配置寄存器使用CC模式,再验证是否读取出来的温度有差异.