Dear Expert
请问一下现在设定成判据是5mA,以这个评估板为例,实际在多大电流范围会产生动作?
Datasheet中5mA、10mA、30mA、50mA是不同的判定点档位,5mA可对应UL943标准,30mA与IEC60364标准相对应。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Expert
请问一下现在设定成判据是5mA,以这个评估板为例,实际在多大电流范围会产生动作?
Datasheet中5mA、10mA、30mA、50mA是不同的判定点档位,5mA可对应UL943标准,30mA与IEC60364标准相对应。
您好,
实际跳闸电流应该与您调试设定的电流一致,数据手册20页第3步说明了接地故障阈值点调节步骤;AFE3010-EVM用户指南3.1.1 Quick Start Setup - Testing the Trip Current也说明了中断故障电流设定步骤。
AFE3010-EVM用户指南:
Dear Amy
这个demo中用的CT,是什么材质的磁芯? 能否提供这个CT的资料?