This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: 关于1843角度分辨率问题

Part Number: AWR1843BOOST


利用网页配置天线参数为4R3T,然后在2维平面上画出很多帧累积的检测点,结果如图。

这个数据可以认为没有目标动,我拿着板子一直晃,然后把所有帧里的点画到xy平面上的结果,感觉水平方位很有规律,有很多射线,两条射线间大概是1.8度,不明白为什么,问题如下:

1.请问大佬为什么雷达检测的点是一条条射线状的,且两条射线间的角度差大概在1.8度?

2.网页上显示的角度分辨率(azimuth res-deg)(15deg+elevation)是啥意思,跟这个结果有啥关系?

我现在大概猜测 4r3t天线中,水平方向2t发挥作用,相当于虚拟了8个接受天线,然后角度分辨率按公式等于2/N弧度,N为天线个数,则大概是14.25度,所以网页标的15度?(上图左上角天线配置azimuth res后面显示15deg+elevation),然后再除以8大概在1.78度,跟两射线间的角度相似.。。不知道有没有道理,感觉就是瞎猜啊。。。

高度方向的zy平面图如下,横坐标为z,纵坐标为y

好像高度方向的角度分辨率没什么规律?

  • 你好,

    我们通常的测试是雷达固定,用角反来当检测目标。分辨率是和收发天线数相关,也是可以通过超分辨算法来提高的。

    在下面的文档里,你可以看可以通过实测两个角反来得到实际支持的角度分辨率(没有使用高阶算法)。

    www.ti.com/.../tiduen5

    4.2.2.1 In-lab Angular Resolution

    Two corner reflectors were placed with an angular separation of approximately 1.5 degrees at a distance of 8 m from the mmwave sensor.