This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: 使用mmWave_Demo_Visualizer 3.5.0测试出的目标分析问题

Part Number: IWR6843


你好!

环境:IWR6843ISK
1.烧写的程序xwr68xx_mmw_demo.bin来自:E:\mmwave_industrial_toolbox_4_5_1\labs\out_of_box_demo\68xx_mmwave_sdk_dsp\prebuilt_binaries
2.使用的GUI:mmWave_Demo_Visualizer 3.5.0
3.雷达放置在支架上,距离学校操场的栏杆大概0.5m.

雷达前方没有目标走动,使用GUI能测试到三个点目标:
1.请问Range Profile里面有很多SNR>15dB的地方,但是测试点只有3个点,是不是其他地方都作为静态杂波被消掉了?
2.另外这3个点为什么没有消掉?大部分是什么原因造成的?是边上的铁丝网被风吹动产生的吗?如何排查?

下面是测试的图