This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
通过"AWR1843BOOST+DCA1000EVM"拿到adc_data.bin文件以后,需要用matlab解析文件得到原始adc数据。
1.swra581b中有关bin文件的解析代码,我们使用的是AWR1642的。但是我没用过matlab,所以就在matlab里面新建了一个脚本,直接把代码copy到matlab里面,改了文件名,但是运行报错。具体怎么使用解析代码在matlab中运行可否简单告知?
2.我在网上找到了别人写的解析代码,与swra581b中已经给出的差别很大,但是matlab可以运行。解析出来以后数据格式是复数形式;我想问,如果使用swra581b给的代码解析bin文件,解析出来的数据格式是什么形式,也是以矩阵形式存在展现出来的复数?如果是,那么复数的实部和虚部分别代表什么意思呢?如果不是,那具体是什么形式?
感谢您的回答!
你好,
解析代码可以参考swra581,错误可以根据maltab提示的错误修正的。你可以参考下面的论坛讨论:
请问你配置的ADC数据是复数,还是是实数? 一般来说,我们设置的ADC为complex x1,接收到的数据是复数的。更多信息请参考:
https://www.ti.com/lit/wp/spyy007/spyy007.pdf
Using a complex-baseband architecture in FMCW radar systems