This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM335: LM335输入电压范围

Part Number: LM335

在数据表中没有找到关于LM335输入电压的范围,请问这款芯片的电压范围是多少?

  • 您好,

    LM335的工作原理相当于一个齐纳二极管,它的击穿电压与温度成10 mV/°K关系。它的工作电流范围是400 μA to 5 mA,具体可查看datasheet 中Figure3

  •  我明白LM335的工作原理相当于一个齐纳二极管,但是齐纳二极管应该只是范围比较大而已,也有一个电压力的范围吧?有没有推荐使用的范围呢?

  • LM335 它的工作是需要提供一个400 μA to 5 mA范围内的电流而工作的,它是以输出电压来标示温度的,换句话说,它的输入参数是电流参数不是电压参数。LM335 工作温度范围是 −40°C to 100°C,根据下图结温25℃时击穿电压约是3V。如果硬要说其工作电压范围,那么其输出电压范围就约为2.35V~ 3.75V