This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: 1843 L3 memory

Part Number: AWR1843


1843 L3 memory  

Can DSS use 2MB of L3 memory?

What shall I do?

A maximum of 768KB of ECC-enabled memory is available as shared DSS_L3 memory in the DSP
subsystem. The memory is structured into sections of 128KB, out of which can be allocated to the DSP or
master Cortex-R4F, as shown in Figure 10-2.

On-chip L3 shared memory of 1024KB, with 512KB dedicated to DSP and 512 KB of memory shared

between the DSP and master subsystems.

DSS_L3RAM 0x5100_0000 0x51FF_FFFF 2MB DSS_L3RAM (L3) shared memory space