你好,Ti。lmp91300调试和烧录有两个问题请教下。
Q1.现在需要调CF的电容,出现个疑问,我写进寄存器的数值无法保存?(我没有尝试烧录其他寄存器的地址,目前只是参考CF电容的调试指南。默认值为什么对不上,这片子给人用过了?)
Q2.INA,的波形有;CF两端的波形呈一条直线,完全没反应。(CF电容100pF~10nF试了几个,没反应。这个可能是什么原因?是板子没焊好吗?)
PS 1.数据写入读取的问题。




2.波形



This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,Ti。lmp91300调试和烧录有两个问题请教下。
Q1.现在需要调CF的电容,出现个疑问,我写进寄存器的数值无法保存?(我没有尝试烧录其他寄存器的地址,目前只是参考CF电容的调试指南。默认值为什么对不上,这片子给人用过了?)
Q2.INA,的波形有;CF两端的波形呈一条直线,完全没反应。(CF电容100pF~10nF试了几个,没反应。这个可能是什么原因?是板子没焊好吗?)
PS 1.数据写入读取的问题。




2.波形



有个疑问,官方的这个烧录的板子到底有没有问题,进行读写操作时,示波器测试SPI几个测试点没有波形变化?我是完全照板子焊的(那几个DNS的没焊,R5只有332R,阻值太小迅速发热)LMP91300_SWIF_EVM_REV2.pdf
A1.建议您确认购买IC最终进货来源是否为TI,建议您使用从正规渠道购买的IC
如果需要购买的话,建议从TI.com官网购买产品
A2,对CF电容的调试,您是按照datasheet中8.2.2.4 CF (CFA and CFB Terminals)章节进行的吗?应该测CFB(17脚)一端,不是CF两端,请注意:由于 CFB 端子对电容负载非常敏感,建议使用有源探头,无源探头的话需串联 1kΩ Ω 电阻
建议将CFB波形和INA波形同时测量显示在同一屏幕内,像datasheet 中Figure21,INA的频率高,INA的频率是CFB的多倍
我对比了下您附的原理图,其中有一些参数与下面用户指南中原理图参数不一致,这应该是造成通信没波形的原因,您尝试用下面中原理图参数调试,看是否可以。
因为TI已经不再对LMP91300做支持,所以这个板子的BOM无法提供,一些问题也只能参考现有帖子的回复去寻找答案
关于产品生命周期,TI有以下政策:
https://www.ti.com.cn/zh-cn/support-quality/quality-policies-procedures/product-life-cycle.html
因为TI已不再对LMP91300做支持,关于它的寿命和替换计划,我再去确认下