Other Parts Discussed in Thread: MMWAVEICBOOST
你好,如截图,运行mmwave_industrial_toolbox_4_7_0\labs\vital_signs\68xx_vital_signs下的gui,点击开始后,命令窗口停止在这一步,gui不显示任何图形数据。请问需要怎么处理?
IWR6843AOPEVM上的芯片丝印是“QGALP”;S1.1= ON,S1.2=ON,S1.3=ON,S1,.4=OFF; S2.1= OFF,S2.2=ON
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,如截图,运行mmwave_industrial_toolbox_4_7_0\labs\vital_signs\68xx_vital_signs下的gui,点击开始后,命令窗口停止在这一步,gui不显示任何图形数据。请问需要怎么处理?
IWR6843AOPEVM上的芯片丝印是“QGALP”;S1.1= ON,S1.2=ON,S1.3=ON,S1,.4=OFF; S2.1= OFF,S2.2=ON
请看一下MMWAVEICBOOST和IWR6843AOPEVM的配置是否按照下面的网站配置的。https://dev.ti.com/tirex/explore/content/mmwave_industrial_toolbox_4_7_0/labs/common/docs/hardware_setup/hw_setup_mmwaveicboost_mode_functional.html
配置没什么问题,请确认一下AOP板子上的SW3是否设成了OFF?
我按照下面user guide里操作了一遍,GUI可以显示。请再按照下面的user guide仔细检查一遍,如烧写的是否是vital_signs_demo_68xx.bin文件,COM口是否和device manager里的COM口一致?
https://dev.ti.com/tirex/explore/node?a=VLyFKFf__2.4.0&node=ALCGDS5qxpkOXRTFNYu87Q__VLyFKFf__LATEST
您可以看一下user guide,使用不同的cfg配置文件,对板子的摆放也有要求。
For initial measurement subject should stay still for 10-15 seconds to allow the application to calibrate. For subsequent measurements the subject must stay still for 5-10 seconds.
For Sensor in Back, the EVM can be placed in the back of a car seat or in a seat cushion. This can be done by placing the EVM in an enclosure as shown below.
请问你的问题解决了吗?我也遇到GUI无显示的问题,front和back cfg文件都没有用
我调用front cfg可以正常显示的;你确认下是否两个硬件都有:MMWAVEICBOOST和IWR6843AOPEVM;然后按照一楼Shine给的链接去配置;两块板子先上电,再打开gui,gui能自动找到正确的串口号应该就可以了。
我只有IWR6843AOPEVM一块板子。一定要MMWAVEICBOOST吗?
按照demo的要求需要MMWAVEICBOOST;你可以尝试把串口引出来,但是我没有试过 - -、