您好,我使用的是mmwcas-rf-evm和mmwcas-dsp-evm,想用这个4chip_cascade_MIMO_example捕获走路的人,设置Cascade_Configuration_MIMO的local nframes_master=500,但还是很快就结束了,捕获不到动态的人,我该修改Cascade_Configuration_MIMO的什么参数才可以呢,我想得到signal_processing_4chip_cascade的这样子的点云,请问我该如何配置参数

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我使用的是mmwcas-rf-evm和mmwcas-dsp-evm,想用这个4chip_cascade_MIMO_example捕获走路的人,设置Cascade_Configuration_MIMO的local nframes_master=500,但还是很快就结束了,捕获不到动态的人,我该修改Cascade_Configuration_MIMO的什么参数才可以呢,我想得到signal_processing_4chip_cascade的这样子的点云,请问我该如何配置参数

你好,
如果你想一直获取frame,可以把number of frame设置为0。也可以继续加大number of frame的值,最大65535。
Number of frames to transmit
16 bit unsigned number
Valid range: 0 to 65535 (0 for infinite frames)
您好,我用这个去测一面墙,如下图我红笔画的部分。墙前面是两个人,墙的点云特别少,请问是什么原因呢?右边时3D点云,左图时点云的俯视图