MMWCAS-DSP-EVM配套MMWCAS-RF-EVM使用,采用开发板自带的sdimage_3_7_1.img.xz,能够跑通《mmwave_studio_cascade_user_guide.pdf》里面的演示例程,查看其内核版本:u-boot 2016.05,linux kernel 4.4.84.根据《VisionSDK_Linux_UserGuide.pdf》的步骤部署内核:采用了psdkla-u-boot-REL_VISION_SDK_03_08_00_00.tar.gz与psdkla-kernel-REL_VISION_SDK_03_08_00_00.tar.gz。并依据其它相关文档做了如下更改:
1、MAKECONFIG=tda2xx_cascade_linux_radar in Rules.make
2、采用/ti_components/os_tools/linux/kernel/linux-kernel-addon下的文件对kernel和u-boot打补丁
3、在uenv.txt文件里修改fdtfile=dra7-cascaderadar-infoadas.dtb
4、修改/etc/network/interfaces /lib/systemd/network/80-container-host0.network /lib/systemd/system/systemd-networkd.service 使其为静态IP
制作SD启动卡,进入系统,出现如下异常打印信息:
Card did not respond to voltage select!
invalid mmc device
Net: Could not get PHY for ethernet@48484000: addr 2
Warning: ethernet@48484000 using MAC address from ROM
eth0: ethernet@48484000
Hit any key to stop autoboot: 0
[ OK ] Started telnetd.service.
[FAILED] Failed to start Network Service.
See 'systemctl status systemd-networkd.service' for details.
[ OK ] Stopped Network Service.
Starting Network Service...
[ OK ] Started Login Service.
[FAILED] Failed to start Network Service.
See 'systemctl status systemd-networkd.service' for details.
[ OK ] Stopped Network Service.
Starting Network Service...
[FAILED] Failed to start Network Service.
See 'systemctl status systemd-networkd.service' for details.
[ OK ] Stopped Network Service.
Starting Network Service...
[FAILED] Failed to start Network Service.
See 'systemctl status systemd-networkd.service' for details.
[ OK ] Stopped Network Service.
[FAILED] Failed to start Network Service.
See 'systemctl status systemd-networkd.service' for details.
进入系统后,无法ping通PC。
然后我采用《PROCESSOR_SDK_CASCADE_RADAR_03_08_00_00_Binaries_setupwin.exe》里提供的vision_sdk\prebuilt\linux\tda2xx_cascade_linux_radar\hlos\linux\boot里的文件,也出现上述一样的问题。
请问这个问题该如何解决呢,谢谢。