This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: 有关外部主机如何与awr2243通信的问题

Part Number: AWR2243
Other Parts Discussed in Thread: MMWAVE-DFP,

背景:我们是基于AWR2243芯片进行了硬件开发板开发(没有ARM端),外部主机(上位机)通过SPI转USB转接器与AWR2243进行通信

1.之前在官网进行技术咨询回复说,外部主机可以通过调用mmWaveLink库与2243进行通信,我在mmWave-dfp-user-guide中也看到外部主机PC需要通过mmwl_port_ftdi.lib(For single chip systems)或者mmwl_port_ethernet.lib(For cascade chip systems)与2243进行通信,那具体pc端应该怎么与2243通信,需要两个库都调用吗?但外部主机同时只能调用一个库进行通信,我很疑惑

  • mmwl_port_ftdi.lib用在单芯片SPI通信,mmwl_port_ethernet.lib用在多芯片级联网口通信。


  • 我们是基于AWR2243芯片进行了硬件板卡开发,pc机通过自购的USB转SPI工具与2243自研开发板进行通信,关于几个上位机软件与2243通信的问题进行咨询
    1.在mmwave-dfp中提供了单芯片驱动控制库(mmwl-port-ftdi.lib),这个库是否必须和ft4232配置使用,如果用我们自购的USB转SPI工具(自带驱动API),上位机与2243通信时,能否用转换工具自带的api替代mmwl-port-ftdi.lib?还是mmwl-port-ftdi.lib是不依赖于ft4232的通用库?
    2.PC端上位机与2243通信时,是否需要同时调用(mmwl-port-ftdi.lib或者自购转换器api库)+ mmwaveLink库进行2243实时配置?
    3.我们上位机是c#开发,有没有c#方面的调用例子可供参考?

    针对以上问题还有2个点需要补充下:

    4.我们自研开发的基于2243芯片的开发板中没有官网AWR2243BOOST开发板中的arm模块或者DSP模块,这样会不会影响Pc端调用mmWaveLink库;

    5.是否支持外部PC端直接通过SPI转USB工具发送按mmWave-radarICD通信协议组成的协议数据到2243芯片的方式进行芯片配置,非常谢谢

  • 而且我们自研的基于AWR2243的开发板不用ft4432或者是TDA2XXX以及DCA1000

  • 你好,

    建议你把默认代码里SPI相关的库(mmwl-port-ftdi.lib)和代码替换为你们购买的这个usb转SPI的相关库和控制代码。