This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC1004: 如何设置CAPDAC ,如何做offset校准

Part Number: FDC1004


在Page 5,有ERR (Absolute error ,after offset calibration )  ,如何对offset 校准?出厂前是否已经校准?

另外 CAPDAC ,可以设置约0~100pf ,如果我的测试cap约20pf ,我的CAPDAC 应该设置什么样的数值? 我认为可以在6~29pf之间的数据都可以 ,但究竟该选择那个?

  • 我的联系电话13817775946

  • 您好,

    1、电容offset可能是由许多因素造成的,包括传感器的初始电容,板迹线的寄生电容以及传感器和 FDC 之间任何其他连接的电容。FDC1004 的寄生电容在生产时校准完毕,如果系统中存在其他offset源,则需要在应用中校准系统offset电容。可参考下面方法进行校准:

    https://www.ti.com.cn/cn/lit/an/snoa958/snoa958.pdf

    2、您要测得电容范围是什么?CAPDAC就相当于调节输入共模或失调使得需要测量的电容范围都落在 FDC1004 满量程范围 ±15 pF内。比如说输入管脚的电容(包括寄生电容等一切电容)范围是20pF~30pF,那么您就可以将CAPDAC设置为20pF,使输出读数接近 0pf,然后保持此 CAPDAC 值恒定并改变输入电容, 从 20pF 到 30pF, 输出将从 0pf ~ 10pF跟随变化