This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: 在mmstudio中如何配置TDM

Part Number: IWR1843BOOST


根据TI文档 MIMO RADAR(https://www.ti.com/lit/an/swra554a/swra554a.pdf)中提到的TDM-MIMO模式。我在mmstudio中配置的时候出现了一些问题。

我的需求是让3个TX以TDM的模式发送相同的chirp信号

1. 我先定义了一个profile。点击set

2. 然后当我定义chirp的时候。我在"chirp manager"的界面下配置了3个chirp。分别单独允许T0,T1,T2发送。然后我点击“activate”。但是当我再次点击进入该页面,之前的配置就消失了。但我仍点击了set

3. 然后在Frame中的“start chirp TX”和“End chirp TX”中分别设置了0和2。

我的问题是:

>  我的3个操作步骤是否有效,可以实现TDM MIMO。

> 我采集的数据中,我该如何在接收数据中,区分3根发送天线的序号,即我不知道3根天线的发送时序。(比如说:发送顺序是3根天线轮流发送一整个帧,还是在 No of  Chirp loops中设置的chirp数量为总和的情况下,3个天线轮流发送,发到loops的数量时候停止,停在哪根天线算哪根)