Other Parts Discussed in Thread: IWR1642
刚新买了一块1642的开发板,上手先想试试例程,但是烧录后在Visualizer中没有什么现象呢,想请教下是为什么?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
刚新买了一块1642的开发板,上手先想试试例程,但是烧录后在Visualizer中没有什么现象呢,想请教下是为什么?

请问您的芯片版本是多少?SDK3.5只适用于ES2.0
NOTE: ES2.0 devices only This version of the mmWave Demo lab will work only with xWR1642BOOST ES2.0 EVMs, which require mmWave SDK version 2.0 or above. These EVMs are marked with a sticker which says "ES2.0". EVMs which do not have this sticker have ES1.0 devices and require mmWave SDK version 1.xx.xx.xx.
以下链接的步骤参考看一下:
https://dev.ti.com/tirex/explore/node?node=AI-oBzu9O7ZD9w8V94SbBw__VLyFKFf__LATEST
请问怎么分辨呢?文件里面没有给出方法啊?我的芯片上依次写着:
IWR1642
QG
86ZC999
502AC
ABL G1
烧写成功之后,sop2上的跳帽拿掉了吗?
Power off the board and remove the jumper from only header SOP2. Power the board back on (this puts the board back in functional mode)