This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好:
能否同时使用两个天线TX1和TX2,发射两个频段不同的信号S1和S2;接收天线RX1接收到的为S1+S2,只用TX1的发射信号S1去进行去斜,把RX1中的S2分量去掉。能否利用AWR1843BOOST来实现这个实验。
期待您的回答。
你好,
你可以参考xWR1642/xwr6843 mmw demo里的bpm的参考cfg配置。
例如:mmwave_sdk_03_05_00_04\packages\ti\demo\xwr16xx\mmw\profiles\profile_2d_bpm.cfg
你好,
如果你使用的是AWR1843BOOST,请使用TX0,TX2来测试BPM模式。是的,BPM模式只改变相位。
你配置的地方不正确。请参考下面的论坛讨论:
https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/968687/iwr1642boost-mmwave-studio-how-to-config-correct-bpm-mode
你好,感谢您的解答,我已经知道如何配置BPM模式了。
但是我又有一个新的问题:假如我想同时让TX0发射77-78GHz的信号、让TX1发射78-79GHz的信号,能不能实现呢。是否需要自己编程来实现这种方式,如果编程可以实现的话,那么是否有类似的编程例子可以参考呢?
期待您的解答,谢谢~~
你好,
如果我采用4片级联的AWR2243EVM,是否可以利用不同的芯片上的天线,同时发射不同频率的信号呢。比如说4片芯片分别为chip1-chip4,是否可以利用chip1上的TX1和chip2上的TX1同时发射不同频率的信号。
你好,
在这种同时发射不同频率信号的情况下,假设chip1-chip4的第一个发射天线TX1发射出的不同信号为S1-S4,chip1的RX1接收到的为S1+S2+S3+S4,在后续混频处理时,是用chip1的TX1的发射波形S1去进行混频的吗?
若果是这样处理的方式,那么对应chip2的RX1来说,它是否只能用chip2的TX2发射的波形S2去进行混频吗?
这是级联方案的示意图,当chip2-chip4的第一个发射天线即TX4、TX7、TX10同时发射信号时,chip4的接收天线RX13的回波信号为上述三路信号空间延时之和。按照您的说法,那么是否该回波信号只能用TX10来进行混频吗?
但是如果这样的话,在这3发1收的模式下,只能得到一个虚拟阵元的数据,即TX10与RX13间的虚拟阵元,不知道我这样理解是否正确。
感谢您的耐心解答~~