This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: 角度分辨率问题

Part Number: AWR2243


按照TI的MIMO radar手册里面给出的角度分辨率公式:如图

角度分辨率=2/N(弧度)=360/(N*pi)(角度)

 在AWR2243 4芯片级联开发板手册中给出了MIMO模式下和BF模式下的性能参数,如下图:

对于MIMO来说  N=86(192个虚拟天线,去冗余),折算MIMO角度分辨率为1.3与文档给的1.4差不多。

但是对于BF模式来说 N=16;则BF角度分辨率=7° 远大于手册给出的1.4° 。

请问手册上BF模式给出的1.4°是怎么来的,其中with multiple beam steering 代表什么意思