This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE: AWR2243: mmWave Studio 03.00.00.14版本软件启动出错



好的,谢谢,我们现在换了一台电脑可以启动测试,我们在测试中发现一个问题再咨询下您,我们在SPI连接的时候,用示波器采了下m0si上面的数据,发现在打开SPI连接的时候,发给2243的数据先是8个字(0x5678 0x8765 0xFFFF 0xFFFF 0xFFFF 0xFFFF 0xFFFF 0xFFFF),见下图中前8个数据,这个icd文件里有说明,但是隔了一定时间之后,又给2243发了一定个数的0xffff(见图中后半部分),这个在icd文件中没有说明,请问下发一定数量的0xffff字是什么作用,谢谢

  • 根据icd文档,请问后面第5步里的IRQ line变低了吗?

    4. Host writes CNYS (SYNC word = 0x5678 0x8765) and Dummy bytes (0xFFFF 0xFFFF 0xFFFF 0xFFFF 0xFFFF 0xFFFF) on communication channel

    5. Host waits for low on Host IRQ line
    a. If Host IRQ line is low, go to Step 6
    b. If Retry Time expires, Flag Error