Other Parts Discussed in Thread: AWR2243
请问使用脚本使用哪个函数可以修改级联雷达(AWR2243)的发射天线和接收天线的增益。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问使用脚本使用哪个函数可以修改级联雷达(AWR2243)的发射天线和接收天线的增益。
你好,
请问是使用mmwave stuido的LUA么?请通过ar1.ProfileConfig_mult里的参数设定。
>help ar1.ProfileConfig_mult
Int32 ar1.ProfileConfig_mult(UInt16 RadarDeviceId, UInt16 profileId, Single startFreqConst, Single idleTimeConst, Single adcStartTimeConst, Single rampEndTime, UInt32 tx0OutPowerBackoffCode, UInt32 tx1OutPowerBackoffCode, UInt32 tx2OutPowerBackoffCode, Single tx0PhaseShifter, Single tx1PhaseShifter, Single tx2PhaseShifter, Single freqSlopeConst, Single txStartTime, UInt16 numAdcSamples, UInt16 digOutSampleRate, UInt32 hpfCornerFreq1, UInt32 hpfCornerFreq2, Char rxGain) - Profile configuration API which defines chirp profile parameters
_I_ UInt16 RadarDeviceId - Radar Device Id
_I_ UInt16 profileId - Chirp Profile Id [0 to 3]
_I_ Single startFreqConst - Chirp Start Frequency in GHz
_I_ Single idleTimeConst - Chirp Idle Time in µs
_I_ Single adcStartTimeConst - Chirp ADC Start Time in µs
_I_ Single rampEndTime - Chirp Ramp End Time in µs
_I_ UInt32 tx0OutPowerBackoffCode - TX0 channel Power Backoff in dB
_I_ UInt32 tx1OutPowerBackoffCode - TX1 channel Power Backoff in dB
_I_ UInt32 tx2OutPowerBackoffCode - TX2 channel Power Backoff in dB
_I_ Single tx0PhaseShifter - TX0 channel Phase Shifter Value in deg
_I_ Single tx1PhaseShifter - TX1 channel Phase Shifter in deg
_I_ Single tx2PhaseShifter - TX2 channel Phase Shifter in deg
_I_ Single freqSlopeConst - Chirp Frequency Slope in MHz/µs
_I_ Single txStartTime - TX Start Time in µs
_I_ UInt16 numAdcSamples - RX Number of Adc Samples
_I_ UInt16 digOutSampleRate - RX Sampling Rate in ksps
_I_ UInt32 hpfCornerFreq1 - RX HPF1 corner frequency,[b15:0 (0x00-175 kHz, 0x01-235 kHz, 0x02-350 kHz, 0x03-700 kHz)] + TxChnCalibSet[b31:16]
_I_ UInt32 hpfCornerFreq2 - RX HPF2 corner frequency,[b15:0 (0x00-350 kHz, 0x01-700 kHz, 0x02-1.4 MHz, 0x03-2.8 MHz)] + ForceVCOSelet[b16] and VCOSelect[b17] , RetainTxCalUpdate[b24] , RetainRxCalLut[b25]
_I_ Char rxGain - RX Gain in dB(b0:5), RF Gain Target(b6:7)values 30dB:00, 33dB:01, 36dB:10, Reserved:11
相当于对于Tx天线只可以减小输出的功率么,且对于Rx天线不能单独调整,只能同时设置同一块芯片的4个RX通道吗?
我之前尝试过设置如下的参数
对应的函数应该是:ar1.SetRfInterRxGainPhFreqConfig
但是在实际运行的过程中发现会报错,也就是此函数无法使用,这是由于此函数只能适配特定的EVM吗
相当于对于Tx天线只可以减小输出的功率么
是的。
对应的函数应该是:ar1.SetRfInterRxGainPhFreqConfig
但是在实际运行的过程中发现会报错,也就是此函数无法使用,这是由于此函数只能适配特定的EVM吗
请问你是在profilecfg配置前设置的么?
mmwave_dfp_02_02_03_01\docs\mmWave-Radar-Interface-Control.pdf
5.5.12 Sub block 0x010B – AWR_DIGITAL_COMP_EST_CONTROL_SB
Issue this API first in the sequence before AWR_PROFILE_CONF_SET_SB API.
我是在其之后配置的,我待会尝试在profilecfg之前配置,然后将结果告知
在profilecfg之前配置的意思是ar1.SetRfInterRxGainPhFreqConfig在lua脚本中应该先于ar1.ProfileConfig_mult函数运行是吗?我做了这样的尝试,但是任然报错,且报错的信息如下。似乎是这个函数并不能使用。
你好,
请尝试ar1.SetRfInterRxGainPhFreqConfig_mult。
Int32 ar1.SetRfInterRxGainPhFreqConfig_mult(UInt16 RadarDeviceId, Char ProfileIndex, Char RxGainCompEn, Char RxPhaseCompEn, Char RxDelayCompEn, Char RxFreqCompEn, Char TxFreqCompEn, Double Rx0DigitalGain, Double Rx1DigitalGain, Double Rx2DigitalGain, Double Rx3DigitalGain, Double Rx0DigitalPhaseShift, Double Rx1DigitalPhaseShift, Double Rx2DigitalPhaseShift, Double Rx3DigitalPhaseShift, Double Rx0DigitalDelay, Double Rx1DigitalDelay, Double Rx2DigitalDelay, Double Rx3DigitalDelay, Double Rx0DigitalFreqShift, Double Rx1DigitalFreqShift, Double Rx2DigitalFreqShift, Double Rx3DigitalFreqShift, Double TX0DigitalFreqShift, Double TX1DigitalFreqShift) - SetRfInterRxGainPhFreqConfig API which used to induce diffwrent gain or phase or frequency offsets on the different RXs, for inter-RX mismatch compensation
_I_ UInt16 RadarDeviceId - Radar device ID
_I_ Char ProfileIndex - Profile Index for which this monitoring cofig applies
_I_ Char RxGainCompEn - RX gain compensation enable
_I_ Char RxPhaseCompEn - RX phase compensation enable
_I_ Char RxDelayCompEn - RX delay compensation enable
_I_ Char RxFreqCompEn - RX frequency compensation enable
_I_ Char TxFreqCompEn - TX frequency compensation enable
_I_ Double Rx0DigitalGain - Rx0 digital gain
_I_ Double Rx1DigitalGain - Rx1 digital gain
_I_ Double Rx2DigitalGain - Rx2 digital gain
_I_ Double Rx3DigitalGain - Rx3 digital gain
_I_ Double Rx0DigitalPhaseShift - Rx0 digital phase shift
_I_ Double Rx1DigitalPhaseShift - Rx1 digital phase shift
_I_ Double Rx2DigitalPhaseShift - Rx2 digital phase shift
_I_ Double Rx3DigitalPhaseShift - Rx3 digital phase shift
_I_ Double Rx0DigitalDelay - Rx0 digital delay
_I_ Double Rx1DigitalDelay - Rx1 digital delay
_I_ Double Rx2DigitalDelay - Rx2 digital delay
_I_ Double Rx3DigitalDelay - Rx3 digital delay
_I_ Double Rx0DigitalFreqShift - Rx0 digital Frequency shift
_I_ Double Rx1DigitalFreqShift - Rx1 digital Frequency shift
_I_ Double Rx2DigitalFreqShift - Rx2 digital Frequency shift
_I_ Double Rx3DigitalFreqShift - Rx3 digital Frequency shift
_I_ Double TX0DigitalFreqShift - Tx0 digital Frequency shift
_I_ Double TX1DigitalFreqShift - Tx1 digital Frequency shift
很遗憾,情况与ar1.SetRfInterRxGainPhFreqConfig一致,也会报错,且报错情况一致
目前看来可能是此函数未适配EVM?
或者我的使用方法有误?
是否有可供参考的脚本?
你好,
请参考下面的论坛讨论:
https://e2e.ti.com/support/sensors-group/sensors/f/sensors-forum/1018493/tidep-01012-the-right-value-of-input-of-ar1-setrfinterrxgainphfreqconfig_mult-in-ar1-api-on-mmwave-studio
这个帖子只是提到了如何获得正确的输入参数,事实上我已经尝试过这种方法了。也就是说我的函数参数应该是正确的,但是在运行脚本的时候仍旧会报错