This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP117: 用户对隐藏寄存器的读写

Part Number: TMP117

tmp117应该有隐藏寄存器,调整测温线性度等操作,作为用户,可不可以对隐藏寄存器进行读和写操作,来调节测温输出?

  • 您好,TMP117本身就是一款精度很高的温度传感器,16bit的分辨率为0.0078度,在-40~85度范围内的典型精度为+0.05度,通常情况下客户不需要进一步校准。

    那么由于本身它的精度就高,收到外部物理条件的影响比如PCB的材料类型,以及厚度等,会造成轻微偏移读数,这是可以使用温度偏移寄存器0x07来纠正这个错误。另外,没有您说的其他隐藏寄存器,所有的寄存器可以参考TMP117 datasheet的register mapping。