This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: Infineon TC397通过SPI与AWR2243通讯问题

Part Number: AWR2243


目的:Infineon TC397通过SPI与AWR2243通讯

1. AWR2243上电后,会产生Host Irq High信号,经软件读取相应的TC397引脚,电平确实被拉高;

2. TC397通过SPI发送Dummy指令: {0x5678U, 0x8765U,0xFFFFU, 0xFFFFU, 0xFFFFU, 0xFFFFU, 0xFFFFU, 0xFFFFU}。

3. Host Irq引脚并没有变为低电平。

TC397的SPI配置如下:

另外,关于第2部,尝试了多种组合,收到的数据如下:

另外,改变发送数据的大小端格式,Dummy指令变为: {0x8765U, 0x5678U, 0xFFFFU, 0xFFFFU, 0xFFFFU, 0xFFFFU, 0xFFFFU, 0xFFFFU}。

实验结果如下:

烦请大神帮忙看一下,问题出在哪里?