This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP102: 高低温IIC有问题,想咨询下建议上拉电阻。

Part Number: TMP102


主机:FPGA

从机:TMP102:

现象:随机发生I2C通讯失败,常温状态下、-15~60℃情况下都有可能发生,异常发生的温度点随机。异常情况从FPGA主机端看是I2C一直在进程中,没有完成一组周期的I2C通讯,异常发生后SCLSDA一直是高电平状态。

正常通讯时的波形:

 

异常通讯时的波形:

 

 

分析:通讯正常时,主机写地址49h,数据00h;主机写地址49h,数据1Ch00h。通讯异常时,波形只有前面4FRAME,少了FRAME 5。怀疑是从机一直未发送这组数据,导致I2C进程卡死。此外,这种I2C进程卡死的情况在I2C上拉电阻为1.5K左右时高概率发生,大概50台里面出现三四台。这些发生异常的产品,我们修改上拉电阻为4.3K后反复做高低温时异常情况不复现。观察到TMP102的数据手册上的拉电阻建议值为5K,因为这组I2C总线上还有一个I2C器件,想询问这种情况下建议上拉电阻值是多少?另外,原厂是否能确认是由于上拉电阻的原因导致I2C进程异常情况的发生的?