This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: 短距离雷达 SRR demo 编译 无法结束

Part Number: IWR1642BOOST


大家好,我在编译SRR DEMO时有时会出现编译无法结束的情况,进度提示在39%左右。下面是编译时的一些输出信息。谢谢!

<Linking>
Finished building target: "srrdemo_16xx_mss.xer4f"

C:/ti/mmwave_sdk_03_05_00_04/packages/scripts/ImageCreator/out2rprc/out2rprc.exe srrdemo_16xx_mss.xer4f srrdemo_16xx_mss.bin
Parsing the input object file, srrdemo_16xx_mss.xer4f.
Appending zeros 0
Appending zeros 256
Appending zeros 83720
File conversion complete!
C:/ti/mmwave_sdk_03_05_00_04/packages/scripts/ImageCreator/multicore_image_generator/MulticoreImageGen.exe LE 37 0x00000006 srrdemo_16xx.bin 0x35510000 srrdemo_16xx_mss.bin 0xb5510000 C:/ti/mmwave_sdk_03_05_00_04/firmware/radarss/xwr16xx_radarss_rprc.bin 0xd5510000 E:/CODE/mmWave Radar/srrdemo_16xx_dss/Debug/srrdemo_16xx_dss.bin