This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243BOOST: AWR2243BOOST设计与CHECKLIST不一致,以哪个为准

Part Number: AWR2243BOOST
Other Parts Discussed in Thread: AWR2243

 2243 DEMO(AWR2243BOOST)  与 CHECKLIST《HardwareDesignChecklist_V0p1_AWR2243_SPRR419》 不一致点,以哪个为准:

1.SYNCIN 下拉电阻因该为多少

    

   DEMO   设计 10K下拉

SYNCIN

100K pull down to GND 

N10

100K pull down to GND

 

CHECKlist  100K

2.VIN_SRAM    VIN_SRAM的去耦电容


DEMO设计0.1uF

VNWA

Connect to 1.2V

P14

0.22 uF decap

VIN_SRAM

Connect to 1.2V

R14

0.22 uF decap

CHECKlist    0.22uF

 

  1. 我们用LP87524供电的时候,用的内部LDO bypass 模式,VOUT_PA对应的这个R87 过电流是多少?